Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Does PSoC 4700S Support Inductive Linear Slider Design – KBA226881

Does PSoC 4700S Support Inductive Linear Slider Design – KBA226881

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: VisonZ_71          Version: **

Translation - Japanese: PSoC® 4700S は、インダクティブ リニア スライダー デザインをサポートしますか - KBA226881 - Community Translated (JA)

Question:

Does PSoC® 4700S support inductive linear slider design?

Answer:

Although the MagSense™ component does not include the linear slider widget, PSoC 4700S series devices can support linear slider design. This is done by combining multiple button widgets, as shown in the following figure.

pastedImage_1.png

Calculate the finger position using the slider centroid algorithm, which is the same algorithm used for self-capacitance sliders. Note that the centroid algorithm must be added manually; the MagSense component does not generate it automatically for button widgets.

To get a separate .c/.h source code file of the slider centroid algorithm, go to https://community.cypress.com/docs/DOC-17145.

0 Likes
373 Views
Contributors