Do Address pins have internal Pull-up or Pull-down circuits?
Anonymous
Not applicable
Mar 07, 2011
02:29 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 07, 2011
02:29 AM
Translation - Japanese: アドレスピンには内部プルアップ、または 内部プルダウンはありますか? - Community Translated (JA)
Question: Do you have internal pullups or pulldowns on your address pins so that they may be left floating?
Answer:
There are no pullups or pulldowns on address pins. If the customer doesn't want to use half of the memory, then any one of the address pins can be tied high or low and the remaining can be used to address the part.
Labels
- Tags:
- async fast srams
- async micropower (mobla) srams
- dual-port srams
- fifos
- mobl dual-ports
- nonvolatile ram
- quadporta dse srams
- synchronous srams
- wafer & die
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous