Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Differential Output Support of Audio DAC in S6J3200 - KBA229319

Differential Output Support of Audio DAC in S6J3200 - KBA229319

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: AmyW_86            Version: **

Translation - Japanese: S6J3200 のオーディオDACの差動出力サポートについて- KBA229319 - Community Translated (JA)

Question:
Does the Audio DAC of S6J3200 support differential output?

Answer:
Yes, the Audio DAC in S6J3200 supports differential output when using the Bridge-tied Load (BTL) method, where the output signals DAC_L and DAC_R have a 180o phase difference. The DAC Polarity Configuration Register (DPCR) of the Audio DAC module should be set to 01b or 10b to reverse the polarity of the upper (Left_DATA) or lower (Right_DATA) 16 bits when BTL is applied.

Figure 1. Example of DAC Differential Output

pastedImage_1.png

For more information about BTL, see S6J3200 Hardware Manual.

0 Likes
298 Views
Contributors