Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Differences between FX2 and FX2LP

Differences between FX2 and FX2LP

Anonymous
Not applicable
Question: What are the differences between the EZ-USB FX2 (CY7C68013) and the new EZ-USB FX2LP (CY7C68013A) products?

 

Answer:

An overview of the feature difference between the FX2 (CY7C68013) and the FX2LP (CY7C68013A), are listed as follows:

- Lower power

- Expanded internal code/data RAM

- ECC generation on GPIF data

- Zero-length IN packets with no firmware intervention and Data PID sequencing

- Additional GPIOs in smaller package (CY7C68015A)

 

For more information refer the application note in the link Migrating From EZ-USB FX2(TM) to EZ-USB FX2LP(TM)

0 Likes
1822 Views
Contributors