Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Difference between count & clock pins of PSoC 3/5 Counter component

Difference between count & clock pins of PSoC 3/5 Counter component

KishoreS_96
Employee
Employee
5 sign-ins 50 replies posted 25 replies posted
Question: What is the difference between count & clock pins of PSoC 3/5 Counter component?

 

Answer:

The UDB based Counter component looks like this:

The signal which has to be counted has to be connected to "count" pin whereas the "clock" pin is to run the Datapath of the UDB. In other words, the input signal "count" is sampled by the "clock" input. So the "clock" input frequency has to be atleast twice that of "count" input signal so that it can be counted properly.

0 Likes
467 Views
Contributors