Community Manager

Community Manager
Jul 01, 2022
06:29 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
Difference between OptiMOS™ 6 and OptiMOS™ 5 in 100V (KA-03463)
OptiMOS™ 6 technology was developed to mainly address high switching frequency applications. The main improvements compared to OptiMOS™ 5 are related to Figure of merits Qg and Qgd which allow lower switching losses. With the new portfolio it is possible to achieve higher efficiency enabling power density and system cost improvement.
Labels
Rate this article: