Default I2C slave address of CY8C20110
Anonymous
Not applicable
Mar 28, 2011
12:10 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 28, 2011
12:10 PM
Question: What is the default I2C slave address of any CapSense Express device?
Answer:
The default I2C slave address for CapSense Express devices is 00h. If there are multiple CapSense Express devices or address of one device need to be changed then please refer to the following KB article: Addressing multiple CapSense Express devices on the same I2C bus.
Labels
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous