Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Debugging PSoC® Devices When the Debug Select Option Is Set to GPIO - KBA91118

Debugging PSoC® Devices When the Debug Select Option Is Set to GPIO - KBA91118

Anonymous
Not applicable
Version: **

 

Question: Is it possible to debug PSoC® 3/ PSoC 4/ PSoC 5LP devices if the Debug Select option in the project_name.cydwr file is set to GPIO?

 

Answer:

It is possible to debug PSoC 3 and PSoC 5LP devices when the Debug Select option in the System tab of the project_name.cydwr file is set to GPIO, but attaching it to the running target is not possible. But in the case of PSoC 4 devices, both debugging and attaching to the running target are not possible if the Debug Select option in the System tab of the project_name.cydwr file is set to GPIO.

0 Likes
531 Views
Contributors