Moderator
Jan 23, 2023
01:19 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jan 23, 2023
01:19 AM
DC Motor system IC TLE9560/1/2 - Why are the drain-source overvoltage thresholds individually configurable high-side and low-sides of the same half-bridge?
In some applications, a current measurement is required for each half-bridges, by inserting a shunt resistor between the source of the low-side and the common SL pin of the MOSFET driver.
The drain-source overvoltage of the low-side monitors the VSHx - VSL where VSHx is the phase voltage of the considered half-bridge.
In general the MOSFETs used for one half-bridge (high-side and low-side) are symmetrical.
The individual configuration of the drain-source overvoltage (DSOV) threshold of the high-side (HS) and of the low-side (LS) enables the compensation of the shunt resistor inserted at the low-side.
For example:
- the nominal Rdson of the HS and LS is 5 mOhm
- the resistance of the shunt resistor inserted in the LS path is 5 mOhm
Selecting DSOV threshold for LS = 2 x DSOV threshold for HS allows the same trigger current for detection of HS DSOV and LS DSOV.
Labels
Rate this article: