Translation - Japanese: サイプレスCyUsb3.sysプログラマーズリファレンス - KBA99226 - Community Translated (JA)
Question:
Where do I get detailed information about Cypress’s CyUsb3.sys driver?
Answer:
CyUsb3.sys is a kernel-mode USB function driver, licensed for distribution ONLY with Cypress USB products and products that employ Cypress USB chips.
A detailed CyUsb3.sys Programmer’s Reference manual (CyUSB.pdf) is available in documentation folder of FX3 SDK. It can be found in the following default SDK installation path:
64-bit Windows:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\SuiteUSB
32-bit Windows:
C:\Program Files\Cypress\EZ-USB FX3 SDK\1.3\doc\SuiteUSB