Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Current consumption at switching frequency 250kHz (2EDN)

Current consumption at switching frequency 250kHz (2EDN)

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

The supply voltage range is written in the 2EDN datasheet under “operating range”. There is a  https://www.infineon.com/cms/en/about-infineon/company/contacts/support/images/1173_Image1.png graph in data sheet which allows an estimation related to the switching voltage level (= 3 .. 12 mA @250kHz including a FET of 1.8nF Qg).
The graph shows values at 25°C ambient temperature with a self-heating device. An external load of 1.8nF generates realistic conditions. For detail calculation, please check the available application notes.

0 Likes
91 Views