Community Manager

Community Manager
Nov 22, 2021
09:47 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
Constant “10” in the Fsw(max) equation - KBA234212
Version: **
The maximum sense clock frequency [Fsw(max)] is calculated as follows:
The selected sense clock frequency should be such that the sensor will charge and discharge completely in each sense clock period. The equation for the maximum sense clock frequency comes from the characteristics of the RC circuit.
In an RC circuit, it takes about 5 RC until the capacitor is completely discharged. Because the discharge is performed in half the time of one cycle, the time of one cycle is T = 2 * 5RC = 10RC; the frequency is calculated as 1 / T; therefore, it is 1/10 RC.
See AN85951 – PSoC™ 4 and PSoC™ 6 MCU CAPSENSE™ design guide for more information.
Labels
- Tags:
- psoc4
Rate this article: