Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Considerations for CapSense Sense Clock Parameters – KBA228329

Considerations for CapSense Sense Clock Parameters – KBA228329

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: AH_96           Version: **

Translation - Japanese: CapSenseセンスクロックパラメーターに関する考慮事項 – KBA228329 - Community Translated (JA)

While developing any CapSense® application, it is important to set the correct parameters such as the sense clock frequency, resolution, and IDAC value noise threshold for optimum performance.

1. Sense clock frequency

The sense clock frequency determines the charge-discharge time of the CapSense sensor. This must be chosen such that the sensors charge and discharge completely. An example of incomplete charging of the sensor is shown in Figure 1. Figure 2 shows the complete charging and discharging of the sensor.

The path to the sensor from the GPIO includes a series resistor that slows down the charging and discharging process of the sensor. The series resistor includes an internal resistance of 500 Ω and an external resistor (recommended value of 560 Ω).

The maximum sense clock frequency is decided by the time constant of this combination.

FSW (maximum) = 1 / 10*RSeriesTotal*CP

   pastedImage_9.png

Figure 1: Incomplete charging and discharging of sensor

pastedImage_8.png

Figure 2: Complete charging and discharging of sensor

The minimum value of the sense clock frequency is limited by the scan time and minimum sense clock frequency supported by that device. The hardware scan time is

Scan Time = ((2N -1) / Modulator clock frequency), where N is the resolution of the widget

The sense clock frequency must be set such that the period of the sense clock is lower than the scan time.

For example, consider a mod clock frequency of 24 MHz and resolution of 6. This gives a scan time of 2.625 µs. Therefore, the sense clock frequency must be at least 381 kHz for the sensor to work.

2. Sense clock source

Sense clock source can be direct, PRS8, or PRS12; some devices support SSCx modes.

Direct clock is a constant frequency source. When this is selected, the sensor switches with the constant frequency clock with the frequency specified by the component configuration window.

Direct clock source has higher radiated noise and therefore, in systems where there are strict limitations on the noise emissions, it is recommended to use pseudo random sequencer (PRS) or spread spectrum clock (SSC) as the clock source. Setting the clock source to PRS or SSC will also reduce the number and width of flat spots.

PRS spreads the clock using the pseudo random sequencer to provide lower radiated noise and improved immunity against external noise. PRS8 spreads the clock using PRS to Modulator clock / 256 and PRS 16 spreads the clock to Modulator clock / 4096.

While setting the clock source to PRS, the following condition must be satisfied:

At least one full PRS polynomial should finish during the scan time. That is,

  ( (2 N − 1) /  ModClk )  ≥  ((2 PRSN −1) /  SnsClk )

Where N is the resolution of the widget, PRSN is the number of bits used for PRS (8 or 12), ModClk is the modulator clock frequency and SnsClk is the average Sense clock frequency.

SSC provides a dithering clock with a center frequency equal to the frequency set in the “sense clock frequency” parameter. There are two conditions that need to be met for setting sense clock source as SSC.

20% of the ratio between the Modulator clock frequency and Sense clock frequency should be greater or equal to the SSC frequency range = 32. That is

160 ≤ (  ModClk  /  SnsClk )

At least one full spread spectrum polynomial should complete during the scan time.

  ((2 N − 1) / ModClk )  ≥  ((2 SSCN −1) / SnsClk )

Where N is the resolution of the widget, SSCN is the number of bits used for SSC (6,7,9 or 10), ModClk is the modulator clock frequency, and SnsClk is the average Sense clock frequency.

For example, if the modulator clock Is 24 MHz and SSC6 is required to be configured, the maximum sense clock possible is 150 kHz.

Since 160 ≤ (24000 /  SnsClk )

The valid value of the sense clock is 93.75 kHz (HFCLK = 24 MHz). Therefore, the resolution that needs to be set to use SSC6 is 14.
Since ((2 N − 1) / 24000)  ≥  ((2 6 − 1) /93.75)

Similarly, if SSC7 must be used, the resolution that needs to be set is 15.

pastedImage_10.png

Figure 3: Frequency spectrum with direct clock

            pastedImage_11.png

Figure 4: Frequency spectrum with PRS8

    pastedImage_12.png

Figure 5: Frequency spectrum with SSC7

When the sense clock source is set to Auto, the algorithm chooses the source in the following order based on the criteria mentioned above:

SSC10

SSC9

SSC7

SSC6

PRS12

PRS8

Direct

To detect the sense clock source, CapSense_GetParam(CapSense_BUTTON0_SNS_CLK_SOURCE_PARAM_ID, &val); API can be used after calling CapSense_Start().

Reference:

PSoC® 4 and PSoC 6 MCU CapSense® Design Guide

PSoC 4 Capacitive Sensing (CapSense®)

0 Likes
954 Views
Contributors