Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Connecting the TEST/I2C_SCL Pin of EZ-USB® HX2VL™ - KBA85448

Connecting the TEST/I2C_SCL Pin of EZ-USB® HX2VL™ - KBA85448

Anonymous
Not applicable
Version: **

 

Question: Do I need pull-up resistors to connect the TEST/I2C_SCL pin of an EZ-USB HX2VL device?

 

Answer:

No, you do not need pull-up resistors to connect the TEST/I2C_SCL pin. TEST/I2C_SCL is a multipurpose pin. If this pin has a pull-up resistor, HX2VL enters TEST mode after RESET is de-asserted (from RESET=0 to RESET=1). HX2VL controls the TEST/I2C and SDA pins to ensure that the I2C protocol spec is followed.

Cypress recommends that you connect the TEST/I2C_SCL pin to the SCL of another IC on the schematic, without the pull-up resistor. HX2VL DVK designs that do not use pull-up resistors have been tested and verified.

0 Likes
378 Views
Contributors