Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Confirmation of the Output Level of the Port Set as the Output Port in Traveo™ S6J3110/3120/3200/3300/3310/3320/3330/3340/3350/3360/3370/3400/3510 Series MCUs - KBA221180

Confirmation of the Output Level of the Port Set as the Output Port in Traveo™ S6J3110/3120/3200/3300/3310/3320/3330/3340/3350/3360/3370/3400/3510 Series MCUs - KBA221180

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: Traveo™ S6J3110/3120/3200/3300/3310/3320/3330/3340/3350/3360/3370/3400/3510シリーズMCUの出力ポートとして設定したポートの出...

Question:

Is it possible to check the current output level when the port is set to output?

Answer:

Yes, you can read the port output level from Port Input Data Register (GPIO_PIDRi) by setting port input as:.

- PPC_PCFGRijj.PIE=1

- GPIO_PORTEN.GPORTEN=1

265 Views
Contributors