Configuring a CY8C201xx Device for Use Either with External Pull-ups or With a Master Operating at Different VDD – KBA80735
Anonymous
Not applicable
Jul 03, 2012
02:06 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jul 03, 2012
02:06 AM
Version: *A
Translation - Japanese: 外部プルアップまたは異なるVDDで動作するマスターのいずれかで使用するためのCY8C201xxデバイスの構成 - KBA80735 - Community Translated (JA)
Question: What action must be taken to use a CY8C201xx device either with external pull-ups or with a master operating at different VDD?
Answer:
The CY8C201xx devices support internal pull-up resistors on I2C lines. Table 1 shows the factory default settings for internal pull-up resistors.
Table 1: Factory Default Values for Internal Pull-Up Setting
Device | Internal Pull-Up (factory default) |
CY8C20111/21 | Disabled |
CY8C201A0 | Enabled |
CY8C20110/80/60/40/42 | Enabled |
The setting for the internal pull-up resistors must match the requirements of the overall design. When the setting is incorrect, the following problems can occur:
- Pull-ups should be sized correctly to meet rise time and IOL requirements in an I2C design. Use of internal pull-ups enabled in combination with external pull-ups in a CapSense® device reduces the effective resistance. Proper bus operation is not guaranteed.
- Consider the scenario in which the CapSense device operates at 3.3 V with internal pull-ups enabled while the master operates at 1.8 V and external pull-ups pull the bus to 1.8 V. Bus voltage (VIH) seen by the master is between 1.8 V and 3.3 V due to the voltage divider formed by internal and external pull-ups. This condition can damage the master device.
In the above scenarios, it is recommended to DISABLE the internal pull-up resistor. This has to be done during the device configuration, before soldering it in the end system. To enable or disable the internal pull-up resistors, configure the I2CDM bit (MSB) in the I2C_ADDR_DM (7Ch) register. For more information, see CY8C201xx : Register Reference Guide.
Labels
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous