Version: **
Question:
What parameters should be used to configure the GPIF-II DLL block on the EZ-USB FX3 part?
Answer:
The GPIF-II block on the EZ-USB FX3 can function in various modes with different clock frequencies. The Delay Locked Loop (DLL) associated with GPIF-II is used to guarantee the timing parameters for the interface in certain operating modes. The main operating modes for GPIF-II can be classified into:
In the two synchronous modes, the supported interface clock range is from 10 MHz to 100 MHz. In general, the DLL is not required to be turned ON when the FX3 is operating in a synchronous mode with an external clock input.
When the GPIF-II is configured in asynchronous mode or in synchronous master mode (PCLK is provided by FX3), the interface timing parameters are satisfied only if the DLL block associated with GPIF II is enabled.
The DLL configuration to be used in a specific application depends on factors such as the interface mode and the clock frequency used. The following sections describe the DLL features and the desired configuration for various interface modes.
Some modes of the GPIF-II operation do not require the DLL. In such a case, the GPIF-II interface works on the basis of an internally generated clock, or an externally input PCLK.
The internal clock is generated from the FX3 SYSCLK which runs at a nominal frequency of 384 MHz using a programmable divider. The divisor used for the clock generation is specified through the CyU3PPibClock_t parameter passed to the CyU3PPibInit() API.
Figure 1: Internal PIB Clock Generation
The DLL takes in the internal PIB clock and/or the external PCLK as inputs, and generates a set of three clocks:
Figure 2: GPIF-II DLL Block Diagram
These three clocks will all have the same frequency, but will have a programmable phase difference between them. The phase difference is achieved by selecting each of these clocks from among a set of 16 different phases of a single clock. The 16 phases supported will differ from each other by 360/16 = 22.5 degrees (differ by 1/16th of the clock period).
The timing parameters for the interface are achieved by selecting a set of relative phase differences that meet the requirements. The DLL can be operated in one of two possible modes:
1.1 Master Mode
When the DLL_MODE (bit 16) of the register is selected as MASTER (0), the DLL block generates the three clock outputs on the basis of the internal clock or the external PCLK. The delay to be applied is determined by the DLL based on feedback inputs.
1.2 Slave Mode
In the Slave Mode, the DLL functions as a programmable slave. The delay applied is determined by the value programmed into bits 26:17 of the DLL_CTRL register. When the DLL is being operated in this mode, it is not required that the DLL will achieve lock to the input clock.
Note: The DLL Master / Slave mode is not to be confused with the GPIF-II Master / Slave modes. Later sections of this document describe the complete DLL configuration to be used for various GPIF-II interfaces
The DLL configuration for both of these modes is done through the PIB_DLL_CTRL register. The fields in this register are shown in Table 1. Recommendations on how these register fields are to be programmed are provided in Section 2.
Table 1: PIB_DLL_CTRL Register Definition
PIB_DLL_CTRL Register Address = 0xE0010028 | ||
Field Name | Bit Range | Description |
ENABLE | 0 | DLL Enable bit 0: DLL is disabled 1: DLL is enabled |
HIGH_FREQ | 1 | Whether the PCLK frequency is high 0: PCLK frequency < 70 MHz 1: PCLK frequency ≥ 70 MHz |
DLL_STAT | 2 | Whether DLL has achieved phase lock 0: DLL has not achieved phase lock 1: DLL has achieved phase lock |
CORE_PHASE | 7:4 | Selects the core clock phase. Please follow recommendation in Table 2. |
SYNC_PHASE | 11:8 | Selects the sync clock phase. Follow the recommendation in Table 2 |
OUTPUT_PHASE | 15:12 | Selects the output clock phase. Follow the recommendation in Table 2 |
DLL_MODE | 16 | DLL mode selection. 0: DLL is in master mode and locks to the input clock 1: DLL is in slave mode and creates delayed versions of input clock |
SLAVE_DELAY | 26:17 | Delay to be applied to the input clock when operating in slave mode. |
SLAVE_MODE | 29:27 | Additional slave mode configuration 000: Master mode operation 111: Slave mode operation Other values are reserved. |
DLL_RESET_N | 30 | Reset control for the DLL. 0: DLL is held in reset. 1: DLL is not in reset |
2. DLL CONFIGURATION
The DLL configuration to be used when the GPIF-II is used to implement various interfaces has been characterized for the FX3 device across various operating voltage and temperature conditions.
Table 2: DLL Configuration for Various Interfaces
DLL Parameter | DLL Parameter GPIF Interface Type | |||
Synchronous Slave (Input PCLK) | Synchronous Master (Output PCLK ≥ 80 MHz) | Synchronous Master (Output PCLK < 80 MHz) | Asynchronous Master/Slave | |
DLL ENABLE | No | Yes | Yes | Yes |
HIGH_FREQ | Don’t care | 1 | 0 | 1 |
CORE_PHASE | Don’t care | 0001 | 1111 | 0000 |
SYNC_PHASE | Don’t care | 0000 | 1111 | 1000 |
OUTPUT_PHASE | Don’t care | 1011 | 1011 | 0000 |
DLL_MODE | Don’t care | Master (0) | Slave (1) | Master (0) |
SLAVE_DELAY | Don’t care | Don’t care | 0x46 | Don’t care |
SLAVE_MODE | Don’t care | 000 | 111 | 000 |
Wait for DLL Lock | No | Yes | No | Yes |
Table 2 shows the DLL configuration that should be chosen when the GPIF-II is implementing various types of interfaces.
2.1 Configuring the DLL
The FX3 firmware library currently does not have any APIs which can fully configure the DLL. The DLL needs to be configured through direct writes to the PIB_DLL_CTRL register. The programming sequence to configure the DLL is shown below.
If any changes are to be made to the DLL configuration at runtime, it is recommended that the entire GPIF-II block be powered down and reinitialized using the CyU3PPibDeinit() and CyU3PPibInit() APIs.