cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Configuration of the Status In (SI) and Status Out (SO) Pins

Anonymous
Not applicable

Configuration of the Status In (SI) and Status Out (SO) Pins

Question: 1)  If I want to use the SO pin as a true output of SI, but the signal it is connected to is pulled up to Vcc during startup, will this affect the configuration of SO? 2) Can I change the state of SO is used during operation? 3) How is the function of the INB(INB+) input and the SI(INB-) input defined?

 

Answer:

The Status Out pin controls the function of the INB/INB+ and the SI/INB- inputs. When SO is tied directly to Vcc, these two pins form INB+ and INB-, a differential line-receiver serial-data input pair. When SO is tied to a normal TTL-load without any pull-ups, then the first pin becomes a single-ended serial line receiver while the second pin becomes a single-ended Status Input pin.

This is done with a sensor circuit connected to the SO pin. It senses how this output is externally connected and changes the mode of INB/INB+ and SI/INB- as a result. This sensory circuit is always active and so it is possible to change the status of SO during operation.

If, for example, there is a pull-up during the start-up or configuration of the system, but that pull-up disappears when the system is loaded, then the state of the two pins INB/INB+ and SI/INB- will change from being a differential pair to two single-ended signals. 

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Dec 19, 2008 12:00 AM
Updated by:
Anonymous
 
Contributors