Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Communication Protocols Support in PSoC® 3, PSoC 4, and PSoC 5LP Bootloader Component - KBA84744

Communication Protocols Support in PSoC® 3, PSoC 4, and PSoC 5LP Bootloader Component - KBA84744

KishoreS_96
Employee
Employee
5 sign-ins 50 replies posted 25 replies posted

Version: *D

Translation - Japanese: PSoC®3、PSoC 4、およびPSoC 5LPブートローダーコンポーネントでの通信プロトコルのサポート - KBA84744 - Community Translated (JA)

Question:

What are the communication protocols supported by PSoC 3, PSoC 4, and PSoC 5LP Bootloader Component? What are the different bootloader hosts that can be used with PSoC 3, PSoC 4, and PSoC 5LP?

Answer:

The various communication protocols supported by the Bootloader Component (v1.50 in PSoC Creator4.0) are :

                                                                                                                                                                                                                                                                                                      

  
Communication
     Protocol
 
  
UDB or SCB
     implementation
 
  
App Note
 
  
Device
 
  
Bootloader Host Project provided
     with App Note
 
  
PSoC 3
 
  
PSoC 4
 
  
PSoC 5LP
 
  
PC
     Application
 
  
PSoC 3
     acting as
     a Host
 
  
PSoC 4
     acting as
     a Host
 
  
PSoC
     5LP
     acting as
     a Host
 
  
I2C
 
  
SCB
 
       
N/A
 
  
Yes
 
  
N/A
 
  
Yes
 
  
N/A
 
  
Yes
 
  
N/A
 
  
I2C
 
  
UDB
 
       
Yes
 
  
N/A
 
  
Yes
 
  
Yes
 
  
Yes1
 
  
No
 
  
Yes
 
  
SPI
 
  
UDB
 
       
Yes
 
  
Yes3
 
  
Yes
 
  
No
 
  
No1
 
  
No
 
  
Yes
 
  
UART
 
  
UDB
 
       
Yes
 
  
Yes
 
  
Yes
 
  
Yes
 
  
No1
 
  
No
 
  
Yes
 
  
USB(HID)
 
  
Fixed function
 
       
Yes
 
  
Yes4
 
  
Yes
 
  
Yes
 
  
N/A
 
  
N/A
 
  
N/A
 

For information on support for custom communication protocols, see the “Adding Bootloader Support” topic in the Component Author Guide (PSoC Creator > Help > Documentation > Component Author Guide) .

Note: PSoC Creator supports bootloading through SCB-based UART and SPI Components in PSoC 4.

1 PSoC 3 can be used as a bootloader host with modifications in the PSoC 5LP-based bootloader host project. However, because PSoC 3 has much lower flash size, a bootloadable project that works with PSoC 5LP may not work with PSoC 3 unless the flash space required by the bootloadable project can fit into PSoC 3’s flash. Therefore, it is recommended to use PSoC 5LP as the Bootloader host instead of PSoC 3.

2 The Application note also explains how to create a Windows-based bootloader host.

3 Application note is not available.

4 Only applicable for PSoC 4200L devices. Application note is not available.

0 Likes
446 Views
Contributors