Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Coexistence Throughput Test

lock attach
Attachments are accessible only for community members.

Coexistence Throughput Test

VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

Introduction


The following blog demonstrates a setup for conducting throughput test with coexistence enabled. The results of the conducted tests are also included thereby demonstrating the advantages of using coexistence. 2-wire SECI is used in this test for exchanging coexistence data among the two Cypress chips. More about SECI could be found in the following link: Overview of SECI.

The applications and the platforms used for throughput test are :

  1. Iperf application running in CYW943907WAE4
  2. Le_COC throughput application running in CYW20719Q40EVB_01(attached)

Connections


The diagram below depicts the pins and connections between the two boards:

image1.png

Setting up CYW20719Q40EVB_01:


Any of the available(pins that are brought out in the platform) LHL GPIO pins can be configured to function as SECI. The LHL GPIOs WICED_P10 and WICED_P06(mapped to A0 and D8 respectively on CYW20719Q40EVB_01 ) are used as BT_SECI_OUT and BT_SECI_IN respectively in the attached BT throughput application.

To configure the LHL GPIOs as SECI, the following API is used:

wiced_bt_gpio_select_status_t wiced_hal_gpio_select_function(wiced_bt_gpio_numbers_t pin, wiced_bt_gpio_function_t function);

Eg: for configuring the LHL GPIOs, WICED_P10 and WICED_P06 as BT_SECI_OUT and BT_SECI_IN

wiced_hal_gpio_select_function(WICED_P10 , WICED_GCI_SECI_OUT);

wiced_hal_gpio_select_function(WICED_P06 ,WICED_GCI_SECI_IN );

And finally to enable coexistence in BT, the following API is used:

wiced_result_t wiced_bt_coex_enable( uint32_t seci_baud_rate );

Seci baud rate can be set to a maximum of 4M. In the attached example application, a baudrate of 3M is used.

Eg:

wiced_bt_coex_enable(3000000);

The following code pic depicts the usage of the above mentioned APIs:

bt_coex_code.png

Finally flash the application on the BLE GATT server( CYW20719Q40EVB_01 ), and connect the device to a BLE client. CySmart BLE 4.2 USB dongle was used as the client in this throughput test. Make sure to enable notifications from the server, in the client using the CySmart application.

Setting up CYW943907WAE4 :


Change the last bit/LSB of boardflags parameter in the nvram.txt to 1.

Each boardflags parameter is 32 bit wide. The LSB corresponds to switching the BTCOEX.

Eg;

Boardflag=0x0a0 => boardflags = 0x0a1

Following commands were used to setup the iperf in the AP and STA.

AP as UDP client(tx):

wl mpc 0

wl up

wl frameburst 1

start_ap tput open 0102 6 255.255.255.0 192.168.1.100

iperf -c 192.168.1.101 -u -i1 -t10 -w8m -b10m

AP as TCP client(tx):

iperf -c 192.168.1.101 -i1 -t10 -w8m

STA as UDP  server(rx):

wl mpc 0

wl up

join tput open 0102 192.168.1.101 255.255.255.0 192.168.1.100

iperf -s -u -i1 -8k

STA as TCP  server(rx):

iperf -s -i1 -8k

Finally throughput results here:

BLE and wifi thoughput without coexistence

UDP and TCP without BT interference and coex disabled

wifi data without BT interference and coex enabled

UDP throughput without BLE interference

[ ID] Interval       Transfer     Bandwidth        Jitter Lost/Total Datagrams

[  0] 0.0- 1.0 sec  1.20 MBytes  10.0 Mbits/sec   0.918 ms 0/  853 (0%)

[  0] 1.0- 2.0 sec  1.18 MBytes  9.93 Mbits/sec   0.949 ms 6/  850 (0.71%)

[  0] 2.0- 3.0 sec  1.19 MBytes  9.96 Mbits/sec   1.210 ms 2/  849 (0.24%)

[  0] 3.0- 4.0 sec  1.19 MBytes  10.0 Mbits/sec   0.982 ms 0/  852 (0%)

[  0] 4.0- 5.0 sec  1.19 MBytes  9.95 Mbits/sec   0.984 ms 3/  849 (0.35%)

[  0] 5.0- 6.0 sec  1.19 MBytes  9.97 Mbits/sec   1.407 ms 2/  850 (0.24%)

[  0] 6.0- 7.0 sec  1.18 MBytes  9.89 Mbits/sec   1.526 ms 4/  845 (0.47%)

[  0] 7.0- 8.0 sec  1.19 MBytes  9.95 Mbits/sec   1.005 ms 10/  856 (1.2%)

[  0] 8.0- 9.0 sec  1.19 MBytes  10.0 Mbits/sec   1.134 ms 0/  850 (0%)

[  0] 9.0-10.0 sec  1.19 MBytes  9.97 Mbits/sec   0.790 ms 3/  851 (0.35%)

[  0] 0.0-10.0 sec  11.9 MBytes  9.95 Mbits/sec   1.179 ms 31/ 8507 (0.36%)

pastedImage_2.png

TCP throughput without BLE interference and coex disabled

[  0]  0.0- 1.0 sec  1.01 MBytes  8.47 Mbits/sec

[  0]  1.0- 2.0 sec  1.12 MBytes  9.36 Mbits/sec

[  0]  2.0- 3.0 sec  1020 KBytes  8.36 Mbits/sec

[  0]  3.0- 4.0 sec   947 KBytes  7.76 Mbits/sec

[  0]  4.0- 5.0 sec   859 KBytes  7.04 Mbits/sec

[  0]  5.0- 6.0 sec  1.11 MBytes  9.31 Mbits/sec

[  0]  6.0- 7.0 sec  24.4 KBytes   200 Kbits/sec

[  0]  7.0- 8.0 sec  14.3 KBytes   117 Kbits/sec

[  0]  8.0- 9.0 sec  9.98 KBytes  81.8 Kbits/sec

[  0]  9.0-10.0 sec  4.28 KBytes  35.0 Kbits/sec

[  0]  0.0-10.8 sec  6.05 MBytes  4.70 Mbits/sec

UDP throughput with BLE interference and coex disabled

[ ID] Interval       Transfer     Bandwidth        Jitter   Lost/Total Datagrams

[  0]  0.0- 1.0 sec   680 KBytes  5.57 Mbits/sec   4.734 ms  166/  640 (26%)

[  0]  1.0- 2.0 sec   111 KBytes   906 Kbits/sec   2.146 ms   41/  118 (35%)

[  0]  2.0- 3.0 sec  1.44 KBytes  11.8 Kbits/sec  74.137 ms   30/   31 (97%)

[  0]  3.0- 4.0 sec   375 KBytes  3.07 Mbits/sec   1.105 ms    0/  261 (0%)

[  0]  4.0- 5.0 sec   996 KBytes  8.16 Mbits/sec   3.488 ms   25/  719 (3.5%)

[  0]  5.0- 6.0 sec   291 KBytes  2.39 Mbits/sec   9.384 ms  283/  486 (58%)

[  0]  6.0- 7.0 sec   502 KBytes  4.12 Mbits/sec   6.382 ms    0/  350 (0%)

[  0]  7.0- 8.0 sec   601 KBytes  4.93 Mbits/sec   2.328 ms    5/  424 (1.2%)

[  0]  8.0- 9.0 sec  1.26 MBytes  10.5 Mbits/sec   0.854 ms    4/  901 (0.44%)

[  0]  0.0-10.0 sec  5.86 MBytes  4.94 Mbits/sec   1.252 ms  555/ 4736 (12%)

pastedImage_9.png

Observable packet drops seen in Wifi due to interference from  BLE

TCP throughput with BLE interference

[  0] 0.0- 1.0 sec  29.9 KBytes   245 Kbits/sec

[  0] 1.0- 2.0 sec   369 KBytes  3.03 Mbits/sec

[  0] 2.0- 3.0 sec   605 KBytes  4.96 Mbits/sec

[  0] 3.0- 4.0 sec  21.0 KBytes   172 Kbits/sec

[  0] 4.0- 5.0 sec   247 KBytes  2.03 Mbits/sec

[  0] 5.0- 6.0 sec   490 KBytes  4.01 Mbits/sec

[  0] 6.0- 7.0 sec  9.98 KBytes  81.8 Kbits/sec

[  0] 7.0- 8.0 sec  3.82 KBytes  31.3 Kbits/sec

[  0] 8.0- 9.0 sec  1.89 KBytes  15.5 Kbits/sec

[  0] 9.0-10.0 sec  8.55 KBytes  70.1 Kbits/sec

[  0] 10.0-11.0 sec  0.00 Bytes 0.00 bits/sec

[  0] 11.0-12.0 sec  2.85 KBytes 23.4 Kbits/sec

[  0] 12.0-13.0 sec  1.43 KBytes 11.7 Kbits/sec

[  0] 13.0-14.0 sec  4.28 KBytes 35.0 Kbits/sec

[  0] 0.0-14.3 sec  1.76 MBytes  1.03 Mbits/sec

UDP throughput with coex enabled

[  0] 0.0- 1.0 sec  1.20 MBytes  10.0 Mbits/sec   1.067 ms 0/  853 (0%)

[  0] 1.0- 2.0 sec  1.12 MBytes  9.36 Mbits/sec   0.895 ms 2/  798 (0.25%)

[  0] 2.0- 3.0 sec  1024 KBytes  8.38 Mbits/sec   1.135 ms 21/  734 (2.9%)

[  0] 3.0- 4.0 sec  1.26 MBytes  10.5 Mbits/sec   0.842 ms 2/  898 (0.22%)

[  0] 4.0- 5.0 sec  1.16 MBytes  9.76 Mbits/sec   0.985 ms 8/  838 (0.95%)

[  0] 5.0- 6.0 sec  1002 KBytes  8.21 Mbits/sec   0.952 ms 10/  708 (1.4%)

[  0] 6.0- 7.0 sec  1.40 MBytes  11.7 Mbits/sec   0.944 ms 28/ 1025 (2.7%)

[  0] 7.0- 8.0 sec  1.20 MBytes  10.1 Mbits/sec   1.131 ms 10/  865 (1.2%)

[  0] 8.0- 9.0 sec  1.09 MBytes  9.17 Mbits/sec   1.257 ms 4/  784 (0.51%)

[  0] 9.0-10.0 sec  1.24 MBytes  10.4 Mbits/sec   1.130 ms 25/  912 (2.7%)

[  0] 0.0-10.0 sec  11.6 MBytes  9.75 Mbits/sec   1.435 ms 111/ 8417 (1.3%)

pastedImage_3.png

TCP throughput with coex enabled

[  0] 0.0- 1.0 sec  3.55 MBytes  29.7 Mbits/sec

[  0] 1.0- 2.0 sec  3.61 MBytes  30.3 Mbits/sec

[  0] 2.0- 3.0 sec  3.46 MBytes  29.1 Mbits/sec

[  0] 3.0- 4.0 sec  3.05 MBytes  25.6 Mbits/sec

[  0] 4.0- 5.0 sec  16.4 KBytes   134 Kbits/sec

[  0] 5.0- 6.0 sec  2.14 KBytes  17.5 Kbits/sec

[  0] 6.0- 7.0 sec  2.02 MBytes  16.9 Mbits/sec

[  0] 7.0- 8.0 sec  2.93 MBytes  24.6 Mbits/sec

[  0] 8.0- 9.0 sec  1.42 MBytes  11.9 Mbits/sec

[  0] 9.0-10.0 sec  3.47 MBytes  29.1 Mbits/sec

[  0] 0.0-10.0 sec  23.5 MBytes  19.7 Mbits/sec

BLE throuhgput when coex not enabled

BT_activity_without_coex.png

BLE througput with coex enabled

BT_activity_with _coex.png

Inference:

Given the low priority setting for the BT custom profile(for client-server notification), the throughput saw a observable improvement in WiFi side and at the same time the BT side experienced a heavy throughput loss.

Attachments
1934 Views
Comments
JiCl_3555446
Level 1
Level 1
First like received

Hi VinayakS_26

I tried to reproduce your coexistence setup with a CYW20735 evaluation kit and a slightly different version of the CYW43907 evaluation kit (CYW943907AEVAL1F). The API for the CYW20745 board, it is now :

wiced_bt_coex_enable (uint8_t  seci_in_pin, uint8_t  seci_out_pin)

However, the patch.elf for the CYW20735 file is missing the function wiced_bt_coex_enable despite being in the patch.elf for 20706, 20719 and 20739. I think this is the reason why it does not compile. Do you have any hints on enabling coexistence on these two boards?

VinayakS_26
Moderator
Moderator
Moderator
100 replies posted 50 replies posted 25 replies posted

20735 is a different chip compared to 20706,20719 and 20739.The API wiced_bt_coex_enable() is not yet implemented in the CYW20735.

JiCl_3555446
Level 1
Level 1
First like received

VinayakS_26

Thank you for the reply. I meanwhile purchased a CYW20719 evaluation board. I also have a Wi-Fi board, but it has a slightly different name, CYW943907AEVAL1F. It seems that the CYW943907WAE4 you used is not available for sale.

I debugged some registers in the CYW20719 and I'm very sure ECSI is used to signal things towards Wi-Fi, since the according registers are set. However, I do not get any interrupts from the Wi-Fi chip. I used the WICED Header pins 38+39 on CYW943907AEVAL1F, which seem to correspond to TP18+17 on CYW943907WAE4 according to the schematics.

Is there any further possibility to debug this on the Wi-Fi board?

Is there a specific order to enable coexistence, i.e., do I need to start the Wi-Fi or the Bluetooth board first?

By any chance, could I buy/borrow/... a CYW943907WAE4 board from Cypress?