Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Changing the Target Device (PSoC® 3/PSoC 5LP) in PSoC Creator™ - KBA212590

Changing the Target Device (PSoC® 3/PSoC 5LP) in PSoC Creator™ - KBA212590

Anonymous
Not applicable

Version: **

Translation - Japanese: PSoC Creator™でのターゲットデバイス(PSoC®3 / PSoC 5LP)の変更 - KBA212590 - Community Translated (JA)

Question:

Is it possible to change the target device in PSoC 3/PSoC 5 projects? How do I do this in PSoC Creator?

Answer:

Yes, it is possible to change the target device in a PSoC Creator project.  The target device may be changed anytime during the project development cycle.  In the Workspace Explorer, right-click on the project and select Device Selector.

1.png

Select the new target device from the device selector.

2.png

Note: You also can change the Device Revisions at the bottom.

0 Likes
4054 Views
Contributors