Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CapSense® Tuner Proximity Widget Status Value Change - KBA219115

CapSense® Tuner Proximity Widget Status Value Change - KBA219115

Anonymous
Not applicable

Version: **

Translation - Japanese: CapSense®チューナー近接ウィジェットステータス値の変更 - KBA219115 -Community Translated (JA)

Question:

When does the status signal change for the proximity widget in CapSense tuner?

Answer:

In CapSense tuner for the proximity widget, there are two parameters that determine when the status signal changes.

Proximity Threshold, which detects an approaching hand and Touch Threshold, which indicates a finger touch on the sensor.

  • When the Sensor signal crosses the Proximity Threshold value, the status signal in the tuner will change to 50%. (Sensor signal ≥ Proximity Threshold)
  • When the sensor signal crosses the Touch Threshold, the status signal in the tuner changes to 100% (sensor signal ≥ Touch Threshold)

Note: The CapSense API for proximity—CapSense_IsProximitySensorActive (uint32 widgetId, uint32 proxId)—returns 32 bits of data. In this 32-bit data, only bit[0] and bit[1] indicate the status of the Proximity Threshold and Touch Threshold respectively.

Bits [31..2] is reserved.
Bit [1] indicates that a touch is detected.
Bit [0] indicates that a proximity is detected.

0 Likes
320 Views
Contributors