Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CapSense® Slider and RGB LED Example using the EZ-BLE™ Creator Module – KBA97020

CapSense® Slider and RGB LED Example using the EZ-BLE™ Creator Module – KBA97020

Anonymous
Not applicable

Version: *B

Translation - Japanese: EZ-BLE™ モジュールを使用したCapSense スライダーおよびRGB LEDサンプル – KBA97020- Community Translated (JA)

Question:
Does Cypress provide a CapSense® slider and RGB LED example project for the EZ-BLE Creator Module (CYBLE-022001-00)?

Answer:
Yes, the project can be downloaded along with the user guide from the GitHub location: https://github.com/cypresssemiconductorco/EZ-BLE_PRoC_Module/tree/master/Example_projects


The project can be programmed on the EZ-BLE Creator Evaluation Board (CYBLE-022001-EVAL) plugged on to a BLE Pioneer Kit (CY8CKIT-042-BLE) baseboard.


This project is identical to the example project available as part of the BLE Pioneer Kit (CY8CKIT-042-BLE), the only difference being pin mapping changes. These changes are necessary to accommodate the difference in pin mapping between the CYBLE-022001-EVAL and the CY8CKIT-042-BLE baseboard (explained in the CYBLE-022001-EVAL quick start guide).

Downloading the Example Projects

The following steps should be followed to download the complete project and user guide:

  1. Go to the example project page on github.com and select “CapSense_Slider_and_RGB_LED.zip” as shown in the figure below.

pastedImage_17.png                        

     2.  Select “Raw” button, as shown in the following figure. All the project files and user guide will be downloaded as a .zip file.      
         pastedImage_18.png

Supported Kits and Software

Project

PSoC Creator

Version

Compiler

Development Kits

V3.1 SP2

V3.1 SP1 or lower

GCC

MDK

RVDS

CY8CKIT-042-BLE with CYBLE-022011-EVAL

CY8CKIT-042-BLE with PRoC BLE module (CY5671 or CY5674)

CY8CKIT-042_BLE with PSoC 4 BLE module (CY8CKIT-142 or CY8CKIT-141)

CapSense® Slider and RGB LED Example for
EZ-BLE™ Creator Module

YES

NO

YES

YES

YES

YES

NO

NO

0 Likes
2241 Views
Contributors