cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Can we use multiple LITIX Basic+ ICs with multiple output channels in parallel for Tail/Stop?

MohammedA_41
Employee

Can we use multiple LITIX Basic+ ICs with multiple output channels in parallel for Tail/Stop?

Yes, it is possible to configure multiple LITIX™ Basic+ ICs and its output channels in parallel.

When either Tail or Stop operation is active, only the respective IC which is supplied (supply at VS-pin) will drive the LED group with 100% of nominal current set by RSET. A diode is not needed on the outputs of the ICs as only the ICs which is supplied will provide current to the LED group.
When the combined Tail-Stop operation (both supply signals) is active, both ICs drive the LED group with the a different level of current. This different level of current which is required can be set either with use of PWM signal of via the IN_SET pin (change of RSET value).

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Nov 25, 2021 04:11 AM
Updated by:
 
Contributors