Can the TLE9879_EVALKIT realize a motor design using 3 Hall Sensors?
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Community Translation(JP): TLE9879_EVALKIT は 3 つのホール センサーを使用したモーター設計を実現できますか?
The example BLDC Block Commutation with Hall located in the Arm Pack describes an implementation of a motor using 3 Hall Sensors. Refer to example circled in red https://www.infineon.com/cms/en/about-infineon/company/contacts/support/images/isolar21848_a.png here.
There is also a short description inside this example regarding the correct way to connect the terminals with the sensor outputs and power supplies for the motor, click https://www.infineon.com/cms/en/about-infineon/company/contacts/support/images/isolar21848_b.png here.For guidance on how to use examples, please refer to the instructional videos found here: https://www.infineon.com/cms/en/product/evaluation-boards/tle9879-evalkit Link 1, https://www.infineon.com/cms/en/product/microcontroller/embedded-power-ics-system-on-chip-/?redirId=... link 2.