Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Can Semper S28HS-T/S28HL-T Octal Flash operate in either QPI or QSPI mode? – KBA231294

Can Semper S28HS-T/S28HL-T Octal Flash operate in either QPI or QSPI mode? – KBA231294

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Can Semper S28HS-T/S28HL-T Octal Flash operate in either QPI or QSPI mode? – KBA231294

Author: AlbertB_56           Version: **

There is no provision to support either QPI or QSPI modes of operation.  The Semper™ S28HS-T and S28HL-T  series is a memory device with an octal interface that supports both Octal (x8) Peripheral Interface (OPI), as well as legacy Serial (x1) Peripheral Interface (SPI).  However, the default data bus width setting from the factory is Serial (x1) mode.  Configuration Register-5, bit-0 (CFR5x[0]) is user-defined, in either SPI (x1) mode or OPI (x8) data bus width.  SPI (x1) mode supports SDR (1S-1S-1S) only;  OPI (x8) mode supports both SDR (8S-8S-8S) and DDR (8D-8D-8D).  Therefore, QPI (4-4-4) and QSPI (1-4-4) modes are not supported.

See the following sections in the S28HS-T/S28HL-T datasheet:

  - “Transaction Protocol” for SPI and Octal protocol definitions

  - “Configuration Register 5 - CFR5x” for selection of either SPI (x1) or Octal (x8) modes

  - “Transaction Table” for specific SPI and Octal transition functions, names, and commands

See the condensed Octal Flash datasheet: https://www.cypress.com/file/424156/download

Register for the Semper Access Program to get access to full datasheets, application notes, models, software, and evaluation kits:

    https://www.cypress.com/products/semper-nor-flash-memory

References:

Semper S28HS-T/S28FL-T Octal Flash datasheet (complete): Document Number: 002-18216 Rev. *S

0 Likes
399 Views
Contributors