Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Can I use TLD6098-1EP / TLD6098-2ES for very large output voltage ranges?

Can I use TLD6098-1EP / TLD6098-2ES for very large output voltage ranges?

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

The TLD6098 series can drive output voltages up to 70V. When using dimming, a wide range of output voltages can be driven within one application. Then special care has to be taken for the design of the feedback circuitry. Short-to-ground detection threshold at pin VFB is 100mV and overvoltage threshold at 1.6V. If the minimum output voltage is less than 1/16 of the maximum voltage, then a standard voltage divider is not sufficient.
The solution is to place another resistor from IVCC to VFB extending the output voltage range. Link https://www.infineon.com/cms/en/about-infineon/company/contacts/support/images/ExtendingOVtoS2Gratio... here.
Then the output voltage for a given feedback voltage can be calculated from Kirchoff's current law as:
VOUT = (-(IVCC-VFB)/RFBH2+VFB/RFBL)*RFBH1+VFB.
E.g. when using RFBL = 1 kOhm, RFBH1 = 33 kOhm, RFBHL2 = 68 kOhm, the short to ground detection occurs at 1V at the output and overvoltage is getting triggered at 53V.

0 Likes
104 Views