Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Can BGA614 support a frequency of 4 kHz?

Can BGA614 support a frequency of 4 kHz?

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted
BGA614 can support a frequency of 4 kHz, the only parameter shown from approx. 50MHz onwards is NF over frequency on page 8. Device specification gives the option to run it down to DC.
[Here is the BGA614 datasheet]https://www.infineon.com/dgdl/Infineon-BGA614-DS-v02_01-en.pdf?fileId=db3a304314dca3890115418ffd351...
The background is the measurement setup, which uses bias T to supply the bias current to the transistor and to remove DC from the connector at the signal generator (those devices can get damaged by DC). With this, it is not possible to measure the device performance any longer at the lowest frequency range.
0 Likes
31 Views
Contributors