Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CYW20706 as a Peripheral Device: Multi-connection Support - KBA229331

lock attach
Attachments are accessible only for community members.

CYW20706 as a Peripheral Device: Multi-connection Support - KBA229331

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Version: **

Translation - Japanese: ペリフェラルとしてのCYW20706:マルチ接続サポート - KBA229331 - Community Translated (JA)

CYW20706 can support multi-connection as a Peripheral device. To realize the multi-connection functionality, you need to restart advertising after a connection is established with a Central device. CYW20706 will maintain the current connection and can be scanned and connected by other Central devices at the same time.

The attached hello_sensor example demonstrates how to realize the multi-connection function.

Change the hello_sensor application as follows:

1. In the hello_sensor.c file, add the following API to hello_sensor_gatts_connection_up function to stop and restart advertising:

result = wiced_bt_start_advertisements( BTM_BLE_ADVERT_OFF, 0, NULL );

result = wiced_bt_start_advertisements( BTM_BLE_ADVERT_UNDIRECTED_HIGH, 0, NULL );

2. In the wiced_bt_cfg.c file, change the server_max_links parameter to allow multi-connection. The default value is ‘1’ (single connection); change it to the number of Central devices that the device can connect to.

Note that there is no maximum value for the number of connections, but it is limited by the memory and PHY. The hello_sensor application can connect steadily with up to four Central devices (tested with the CySmart app on phone). There might be packet drops and reduction in throughput because of collision of connection intervals.

See the attached project based on the hello_sensor demo for multi-connection.

Attachments
0 Likes
294 Views
Contributors