Tip / ログイン to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CY8CKIT-025を使用したダイオード温度測定 - KBA97948 - Community Translated (JA)

CY8CKIT-025を使用したダイオード温度測定 - KBA97948 - Community Translated (JA)

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Community Translated by NoTa_4591161          Version: **

Translation - English: Diode Temperature Measurement Using CY8CKIT-025 - KBA97948

質問:

CY8CKIT-025のダイオード温度測定は、両方のダイオードが取り付けられている場合にのみ正しい温度を示します。それはなぜでしょうか?

回答:

キットに同梱されているトランジスタのベースとコレクタは、ユーザーガイドのセクション3.3.4で指定されているようにはんだ付けされていません。温度測定にダイオードを使用するには、キットのユーザーガイドで説明されているように、トランジスタのベース端子とコレクタ端子をはんだ付けしてください。そうでない場合は、両方のダイオード(少なくともエミッターのショートワイヤー(J8 3-4J8 7-8))を取り付けて、ダイオードの温度を正しくする必要があります。両方のダイオードを取り付ける場合には、一方のダイオードのエミッターショートワイヤーがもう一方のダイオードのベースとコレクタを短絡させます。

0 件の賞賛
201 件の閲覧回数
寄稿者