Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CY3640 USB Starter Kit

CY3640 USB Starter Kit

Anonymous
Not applicable
Question: What is the CY3640 USB Starter Kit? What is included in the CY3640 USB Starter Kit?

 

Answer:

The CY3640 USB Starter Kit was designed to serve as an easily customizable platform for USB device development using Cypress' CY7C630xx/631xx USB controllers. This kit is no longer available.

The contents of the CY3640 Development kit are listed below.

Hardware:

  •   Three CY7C63001 Cypress USB Controller devices (One pre-programmed windowed
      controller on the CY3640 USB Thermometer Demo board, and two spare devices (one
      windowed and one OTP)
  •   One Cypress USB Programmer from HI-LO Systems with a wall power adapter, a serial cable
      and programming software on a floppy disk
  •   One CY3640 USB Starter Kit printed circuit board
  •   One low-speed unshielded USB "A to B" Cable
  •   One Cypress USB Starter Kit CD-ROM

Software:

  •   CYASM: Cypress USB controller assembler
  •   USB Thermometer device assembly source code
  •   USB Thermometer Windows application program executable code
  •   USB Thermometer device driver

Soft Documentation:

  •   Cypress USB controller family datasheets
  •   USB Thermometer User's Guide and Application Note: Designing a USB Thermometer with the CY7C63001 USB Controller
  •   USB Thermometer PC board layout and schematics
  •   USB Specification v1.0
  •   Cypress CYASM assembler manual
  •   Cypress USB-related application notes
  •   Cypress databook

Printed documentation:

  •   USB Starter Kit User's Guide
  •   USB Starter Kit Application Note
  •   Registration card
0 Likes
574 Views
Contributors