CY22395 Programmable Drive Strength
Anonymous
Not applicable
Dec 19, 2008
12:00 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Dec 19, 2008
12:00 AM
Question: CYCLOCKsRT gives option for Programmable Drive Strengths with the CY22395. What are the minimum and maximum values, and what do they cross into current values?
Answer:
The maximum value Drive Strength is set by default to 01 (Medium Low) for a 3.3V and 10 for 2.5V (Medium High). This crosses into a minimum 15 mA and a maximum of 23 mA. These should correspond to the ranges obtained by the High and Low drive strength settings.
- Tags:
- clock generation
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous