Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CR Trimming Data in S6E1C1/C3 Series is Erased by Erasing SA0 with Sector Erase Command - KBA226781

CR Trimming Data in S6E1C1/C3 Series is Erased by Erasing SA0 with Sector Erase Command - KBA226781

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: TakashiM_61          Version: **

Translation - Japanese: S6E1C1/C3シリーズのCRトリミングデータは、セクター消去コマンドでSA0を消去すると消去されます - KBA226781 - Community Translated (JA)

Question:

Why is CR Trimming data in S6E1C1/C3 Series 32-Bit MCU (FM0+ Family) erased when SA0 is erased with Sector Erase Command?

Answer:

This is because the 16-byte area from “0x0010_0000” to “0x0010_0010” is synchronized with SA0, and CR trimming data is allocated in this 16-byte area (mapped at the address “0x0010_0004”). Therefore, if Sector Erase Command is executed against SA0, CR trimming data is erased.

Here is an example of Address and Sector Structure of 64 Kbyte Flash Memory in S6E1C/C3 Series.

pastedImage_4.png

0 Likes
248 Views
Contributors