Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CCG3PA Resistor Divider Network in Direct Feedback: Design Guidelines - KBA31220

CCG3PA Resistor Divider Network in Direct Feedback: Design Guidelines - KBA31220

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: YiZ_31           Version: **

Translation - Japanese: 直接フィードバックにおけるCCG3PA抵抗分割のネットワーク:設計ガイドライン - KBA31220 - Community Translated (JA)

In direct feedback applications, CCG3PA uses an IDAC connected to the Feedback pin of DC-to-DC to control the converter’s output voltage. Whenever a change in VBUS voltage is needed, CCG3PA will either source or sink a proportional current at the feedback node, based on the amount of voltage change needed. When the default value of VBUS upon power up is 5 V, the feedback pin of CCG3PA should be close to 1.2 V.

Capture.PNG

Figure 1. Two-Resistor Divider

For converters that have the same default feedback target voltage of 1.2 V, a two-resistor divider network is needed. Because the PPS voltage step should be 20 mV, R1 should be 20 mV/0.1 uA= 200 kΩ. When R1 is resolved, R2 could be calculated from the equation VFB=(5V*R2)/(R1+R2). The recommended value for R2 is 68 kΩ.

Capture.PNG

Figure 2. Three-Resistor Divider

For converters that have a lower feedback target voltage such as TI LM5175, TI LM5176, TI LM34396, a three-resistor divider network is needed. R1 should still be 200 kΩ because of the PPS voltage step requirement. If the feedback target voltage of DCDC is Vref,  you should set the correct value for R2 and R3 so that VFB(CCG3PA)=1.2 and VFB(DCDC) = Vref. Solve these two equations and you get:

R2=63157.894 – 52631.833* Vref

R3= 52631.833*Vref

Some common used values of resistors based on different reference voltages are listed in Table.1.

Vref (V)

R1 (kΩ)

R2 (kΩ)

R3 (kΩ)

Default VBUS value (V)

0.6

200

31.6

31.6

4.997

0.7

200

26.1

36.5

5.036

0.8

200

21

42.2

4.990

0.9

200

15.8

47.5

4.989

1.0

200

10.5

52.3

5.025

Table 1. Quick Reference Table

For the more information about CCG3PA power adapter design, please refer to AN218238.                                                                                                                            

0 Likes
242 Views
Contributors