CAN Interface Interrupt Response Time in Traveo S6J3120 Series MCUs - KBA226514
Employee
Feb 27, 2019
01:06 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Feb 27, 2019
01:06 AM
Author: shusakus_56 Version: **
Translation - Japanese: Traveo S6J3120シリーズMCUのCANインターフェイスの割り込み応答時間 - KBA226514 - Community Translated (JA)
Question:
How long is the CAN interface interrupt response time in Traveo™ S6J3120 series MCUs, under the operating conditions - CPU clock = 112 MHz, IRC clock = 28 MHz?
Answer:
The result of measuring the cycle from "Interrupt factor setting" to "ISR handler activation" was about 455 ns (51 cycle at CPU clock).
Labels
Rate this article: