Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Build CCG4M Project Using CCG4 Project in SDK 3.0.1 and Later Versions – KBA219845

lock attach
Attachments are accessible only for community members.

Build CCG4M Project Using CCG4 Project in SDK 3.0.1 and Later Versions – KBA219845

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: SDK 3.0.1 またはそれ以降に含まれている CCG4 プロジェクトを使用して CCG4M プロジェクトをビルドする - KBA219845 - Community Translated (JA)

1. Question: Does EZ-PD SDK support example projects for CCG4M part numbers?
Answer: No

2. Question: How do I build CCG4M projects using EZ-PD SDK?
Answer: Use the CCG4 notebook project in EZ-PD SDK as a starting point and port it to the CCG4M part.

3. Question: How do I customize CCG4 firmware support to CCG4M based on SDK3.0.1 onwards?
Answer:

  1. Determine the CCG4 and CCG4M part number and pin assignment for firmware.
    CCG4M has two part numbers in the ordering information table in the CCG4M datasheet.

    Part Numbers

    To develop a CYPD4155-96BZXI project, use the CYPD4126-40LQXIT project from the EZ-PD SDK.
    To develop a CYPD4255-96BZXI project, use the CYPD4226-40LQXIT project from the EZ-PD SDK.
  2. In the firmware project, ensure that the I2C Master Component is enabled in TopDesign.cysch.
    Note: For Steps 3 and 4, you can download the datamux_ctrl.c file attached with this KBA and replace the datamux_ctrl.c file under the "solution" folder and ignore Steps 3 and 4.
  3. The USB 3.1 Gen 1/DP1.2 Mux that is internal to the CCG4M part uses the Slave Address 0x54. Change the I2C slave address assigned function in datamux_ctrl.c from 0x10 and 0x11 to 0x54.

    static const uint8_t mux_ps8740_address[NO_OF_TYPEC_PORTS] =
    {
            0x10
    #if CCG_PD_DUALPORT_ENABLE
            ,
    #endif /* CCG_PD_DUALPORT_ENABLE */
    };

    To:

    static const uint8_t mux_ps8740_address[NO_OF_TYPEC_PORTS] =
    {
           0x54
    #if CCG_PD_DUALPORT_ENABLE
           ,
           0x54
    #endif /* CCG_PD_DUALPORT_ENABLE */
    };
  4. Delete/comment all defines/functions for external SS MUX PS8742B and replace the 'Parade' portion of the code to 'Pericom' in the datamux_ctrl.c file
  5. (Additional step for CYPD4155-96BZXI only) If the target part number is CYPD4155-96BZXI, a single Type-C port design, change the target part number to CYPD4126-40LQXIT using the PSoC Creator option as follows before going to Step 6.

    a. Right-click on the project name and use Device Selector to change the part number from CYPD4126-40LQXIT to CYPD4226- 40LQXIT.

    Figure 1. Changing the Target Device with Device Seletor

Figure 1

b. Open TopDesign.cysch, and locate the Bootloadable Component. Use the bootloader binary for the CYPD4226-40LQXIT part instead of the default one, which is for CYPD4126-40LQXIT.

Figure 2
Figure 2

   6. Ensure that pin assignment of each GPIOs on CYPD4155-96BZXI/ CYPD4255-96BZXI device matches the real hardware design. Closely associated with the schematic is the Design Wide Resources (DWR) view, which maps each schematic element to a pin, clock, or hardware block on the CCG4 device. Open the CYPD4126-40LQXI_notebook.cydwr file to see the DWR settings for the project.

Figure 3

As shown in Figure 3, the DWR view has several tabs, which configure aspects such as pin mapping, interrupt mapping, clock selection, and flash security. It is recommended that you restrict any changes to the DWR to the pin mapping view. Do not change the clock, interrupt, system, or flash configurations.

See the following table for GPIO port information versus ball location of CYPD4155-96BZXI/ CYPD4255-96BZXI

Name

CCG4M Ball Location

GPIO Port

VBUS_P_CTRL_P1

K3

P1_6

VBUS_C_CTRL_P1

K4

P1_7

VBUS_DISCHARGE_P1

K8

P2_5

VBUS_P_CTRL_P2

B4

P4_2

VBUS_C_CTRL_P2

B5

P4_1

VBUS_DISCHARGE_P2

B3

P4_3

VCONN_MON_P1/GPIO/VSEL_1_P1

L7

P2_4

SCL_3/VCONN_MON_P2/VSEL_1_P2

L10

P2_7

OVP_TRIP_P1/VSEL_2_P1

K5

P2_1

OVP_TRIP_P2

L8

P3_0

VBUS_MON_P1/GPIO

L4

P2_0

VBUS_MON_P2

B6

P4_0

HPD_P1/GPIO

K7

P2_3

HPD_P2/GPIO

E10

P3_4

GPIO/MUX_CTRL_3_P2

B9

P3_5

GPIO/MUX_CTRL_2_P2

B8

P3_6

GPIO/MUX_CTRL_1_P2

B7

P3_7

VSEL_2_P2/GPIO

H10

P3_1

I2C_SCL_SCB1_EC

L6

P0_1

I2C_SDA_SCB1_EC

K6

P0_0

I2C_INT_EC

L5

P2_2

I2C_SCL_SCB2_AR/GPIO

E2

P1_0

I2C_SDA_SCB2_AR/GPIO

D2

P1_3

I2C_INT_AR_P1

F2

P1_4

I2C_INT_AR_P2

G2

P1_5

SDA_3/GPIO

J10

P2_6

SCL_4

F10

P3_3

SDA_4

G10

P3_2

SWD_IO/AR_RST#

B2

P1_1

SWD_CLK/I2C_CFG_EC

C2

P1_2

7. Save all and rebuild the project.
Two verified examples of CCG4M are available with this KBA (ccg4m_example_projects.zip).
Attachments
1572 Views
Contributors