Bridge Control Panel Result Window Display Error – KBA226069
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Author: VitaS_81 Version: **
Translation - Japanese: ブリッジコントロールパネルの結果ウィンドウの表示エラー– KBA226069 - Community Translated (JA)
Question:
Why is wrong data is displayed in the Result Window of Bridge Control Panel when several commands are available in one line?
Answer:
This is a known issue in Bridge Control Panel v1.19.0 delivered with the PSoC® Programmer™ 3.28.0 tool. When several commands are available in the same line, only the last one is displayed in the Result Window. There is no impact for the commands execution – all commands are performed correctly. This issue will be fixed in the next release of Bridge Control Panel.
In the current release, make sure that each command is written in a separate line to avoid wrong data in the Result Window.