Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Behavior of Wakeup from PSS Mode in Traveo S6J3XXX Series MCUs - KBA222866

Behavior of Wakeup from PSS Mode in Traveo S6J3XXX Series MCUs - KBA222866

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: *A

Translation - Japanese: Traveo S6J3XXXシリーズMCUのPSSモードからのウェイクアップ動作 - KBA222866 - Community Translated (JA)

Question:

How different is the behavior of these Traveo Series MCUs at wakeup from PSS mode by the setting of the power domain (PD)?

Answer:

  1. When the Peripheral Supply Domain (PD2)1 and some of the specified power domains (PD) are OFF in PSS mode, the wakeup reset occurs after the wakeup trigger, and the program starts from bootup.
  2. When the PD21 and some of the specified PD are still ON in PSS mode, the program continues the execution from where it entered PSS mode.

For details on the specified PD that caused wakeup reset when it is OFF in PSS mode, see the section Transition from PSS to RUN in the corresponding hardware manual:

S6J3110: S6J3110 Series 32-bit Microcontroller Traveo™ Family Hardware Manual

S6J3120: S6J3120 Series 32-bit Microcontroller Traveo™ Family Hardware Manual

S6J3200: 32-Bit Microcontroller Traveo™ Family S6J32XX Series Hardware Manual Platform Part

       S6J3300/3350/3360/3370/3400/3510: 32-Bit Microcontroller Traveoä Family S6J33xx, S6J34xx, S6J35xx Se...

Note: This KBA applies to the following series of Traveo MCUs:

  • S6J3110
  • S6J3120
  • S6J3200
  • S6J3300
  • S6J3350
  • S6J3360
  • S6J3370
  • S6J3400
  • S6J3510
455 Views
Contributors