Moderator
Jan 23, 2023
01:35 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jan 23, 2023
01:35 AM
BTN9970: Is operation of HSS OFF & LSS ON and HSS OFF & LSS OFF at 20kHz possible?
Operation with fPWM of 20kHz on INH is not recommended and can reset a thermal shutdown fault condition:
There is the risk the device goes in shutdown (IN=0 and INH = 0). Furthermore in case of a thermal shutdown, the fault condition will be reset with IN and INH low for max 9us. A thermal shutdown condition may not be detected by the system and could lead to thermal overstress and harm ro our device.
Labels
Rate this article: