Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

BTN7030-1EPA: Are protect functions enabled when DEN=0 and EN=1?

BTN7030-1EPA: Are protect functions enabled when DEN=0 and EN=1?

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: BTN7030-1EPA:DEN=0およびEN=1の場合、保護機能は有効になっていますか?

Yes, protection is active if the device is enabled (EN = 1).
If at the same time diagnosis is enabled (DEN = 1), current on the IS pin will:
- mirror the output current (IIS = IOUT/kiLIS)
or
- indicate which fault occurred in the device

0 Likes
170 Views