Moderator
Jan 23, 2023
01:52 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jan 23, 2023
01:52 AM
BRN7030: What is the use case of DEN-pin connected to GND?
The DEN pin enables / disables the diagnsotic function (e.g. open load detection when device is off or current sensing, fault detection when device is on).
For current sensing, EN must be high. If no diagnsotic (e.g. current sensing ) is needed, DEN = low.
For motor control applications I would suggest to enable the diagnostic.
Labels
Rate this article: