Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

BGA Package Difference between 512M and 1G Semper Flash Devices - KBA227835

BGA Package Difference between 512M and 1G Semper Flash Devices - KBA227835

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: PriteshM_61           Version: **

Translation - Japanese: 512Mbitと1GbitのSemperFlashのBGAパッケージの違い - KBA227835- Community Translated (JA)

Question:

What is the difference between 512M and 1G Semper Flash BGA packages?

Answer:

Cypress’ 512M Serial NOR Flash devices (current generation and Semper Flash) support standard 24-ball BGA package. These devices have monolithic die which can fit in a 6mm x 8mm BGA package.

Now, Cypress has introduced the 1G Semper Flash devices with monolithic die. Because of the higher density, 1G monolithic die does not fit into standard 6mm x 8mm Serial NOR 24-ball BGA packages. Therefore, Cypress has introduced a new 8mm x 8mm 24-ball BGA package. As shown in Figure 1, wider BGA-24 package has identical ball placement and signal assignment compared to the 6mm x 8mm 24-ball BGA package, which is compatible with existing boards and enables 1Gb to 4Gb for the respective interface (Quad SPI or Octal or HyperBus™) solutions.

Figure 1. Difference between 512M and 1G BGA Packages (Top View)

KBA.jpg

0 Likes
775 Views
Contributors