Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Assertion Failed - Clang Compiler Exception in PSoC® Creator™ - KBA96713

Assertion Failed - Clang Compiler Exception in PSoC® Creator™ - KBA96713

Anonymous
Not applicable

Version: *A

Translation - Japanese: アサーションの失敗 - PSoC®Creator™におけるClangコンパイラの例外 - KBA96713 - Community Translated (JA)

Question:

Why do I get an “Assertion failed!” error in the code editor of PSoC Creator?

1.png

Answer:

This is a known issue with PSoC Creator. The problem happens only in files that end in a comment and don't contain a newline at the end of the file. To overcome the issue, add a new blank line immediately after one of the following lines at the end of the file.

/*[]*/

OR

/* [] END OF FILE */

The other work around for this issue is to disable semantic parsing from the options dialog in PSoC Creator (Tools > Options > Text Editor > General. > Semantic Parsing

2.png

0 Likes
374 Views
Contributors