Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Alexa Skills Demo

Alexa Skills Demo

MatthewS_51
Employee
Employee
50 questions asked 10 likes received 10 questions asked

This project was created by an extremely talented Cypress Employee: Sri Lakshmi Jayaprakash who is a Sr. Applications Engineer in the Internet, Compute & Wireless Business Unit (ICW).

pastedImage_3.png

 

Project Technology Focuses

  • PSoC® 6 Arm® Cortex®-M4 and Cortex-M0+ MCU
  • CYW4343W 802.11n Wi-Fi + Dual-Mode Bluetooth Radio
  • AWS IoT Cloud Services
  • Amazon Alexa Voice Services
  • Arm Mbed OS

 

Project Requirements

Hardware

Software

 

Project Description

This project leverages a PSoC 6 WiFi-BT Prototyping Kit with Amazon Alexa. An Amazon Echo is used in this project to control the speed of a fan by building a custom skill using the Alexa Skills Kit. The developed custom skill is hosted on the AWS Lambda service. A Lambda function is triggered from Alexa Skills and the function is coded to publish messages to a topic in AWS IoT based on the input from the developed custom Alexa skill. The physical device (PSoC 62 MCU + CYW4343W Wi-Fi/Bluetooth Radio on kit) subscribes to this topic in AWS IoT and generates appropriate PWM signals to control the speed of the fan.

pastedImage_14.png

pastedImage_15.png

pastedImage_16.png

 

Project Links

 

 

Resource List

125712 Views