Accessing PSoC 3/5 Registers in Firmware
Employee
Mar 29, 2011
04:01 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 29, 2011
04:01 PM
Question: How do I access (Read/Write) the Registers of PSoC 3/5 in firmware?
Answer:
To access registers in firmware, use the following functions.
CY_SET_REG8(addr, value);
CY_GET_REG8(addr);
Similarly REG16 & REG32 functions are also there. Please refer to System Referecne Guide for more APIs.
Example:
CY_SET_REG8(CYDEV_IO_PRT_PRT1_DR, 0X01)); // Write the value 1 to Port 1 Data Register.
Port1Register = CY_GET_REG8(CYDEV_IO_PRT_PRT1_DR); // Read the Port 1 Data Register into a Variable "Port1Register"
The macro is defined in the header file, cytypes.h". PSoC 3/5 registers are defined in the header file "cydevice.h"
Labels
Rate this article: