Community Manager

Community Manager
Jul 15, 2022
06:49 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: Why does CAN FD work on the bench but not in the vehicle? – KBA235525
Version: **
The transmitter delay compensation offset is the most common cause of this. For an example of a 2-Mbps CAN FD network, the typical value is 400 ns.
Check the “NTDCRx.TDCO” setting for the AURIX™ TC2xx family and the “TDCRi.TDCO” setting for the AURIX™ TC3xx family.
For more details, see the following sections of the User’s manual:
- For AURIX™ TC2xx devices: “Controller Area Network Controller (MultiCAN+)” section
- For AURIX™ TC3xx devices: “CAN Interface (MCMCAN)” section
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
- Tags:
- Interrupt controller
Rate this article: