Community Manager

Community Manager
Jul 19, 2022
02:53 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: Which pin default state is defined by HWCFG6? – KBA235440
Community Translation:タイトル:AURIX™MCU:どのピンのデフォルト状態がHWCFG6によって定義されていますか? – KBA235440
Version: **
See “Legend” in the “Package and Pinning Definitions” section of the datasheet (DS). HWCFG6 defines the default state of a pin that has “PU1” or “PD1” in the “Type” column. In actual, no device has a pin with “PD1”.
For more details, see the “General Purpose I/O Ports and Peripheral I/O Lines (Ports)” section of the User’s manual.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
- Tags:
- ports
Rate this article: