AURIX™ MCU: What is the meaning of the letters U, SV, E, and SE next to the description of the registers? - KBA234627
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Community Translation: AURIX™ MCU: レジスタの説明の隣にあるU、SV、EおよびSEの文字の意味は何ですか? - KBA234627
Version: **
The letters U, SV, E, and SE represent the access mode of the register as follows:
Letters |
Description |
U |
Access permitted in User mode 0 or 1 (applicable to write and read). |
SV |
Access permitted in Supervisor mode (applicable to write and read). |
E |
ENDINIT protected write. “E” means a write access is only allowed when ENDINIT is inactive (for a short time window) after a correct ENDINIT password unlock sequence as described in the SCU chapter. |
SE |
Safety ENDINIT protected write. “SE” means a write access is only allowed when safety ENDINIT is inactive (for a short time window) after a correct Safety ENDINIT password unlock sequence as described in the SCU chapter. |
For more details, see the Register access modes section in the user’s manual.
- This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series