AURIX™ MCU: What is "code example" and "expert training"? – KBA236006
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Version: **
A “Code Example” or “Expert Training” is a fully working project (for AURIX™ Development Studio (ADS)) that demonstrates how to configure and use one or more modules and features of AURIX™ microcontrollers.
An expert training is composed of two parts:
- Source code
- Tutorial
The source code of each code example is based on Infineon Low Level Drivers (iLLDs) and can be found at Infineon GitHub or directly imported within ADS using the dedicated import function:
File >> Import... >> Infineon >> "AURIX Development Studio Project", select "Infineon Code Examples Repository" and select the code example to be imported.
You can also click Import AURIX Project in the Quick Links view of ADS.
Each component of the code example is explained in the tutorial. The tutorial can be accessed from a dedicated Infineon webpage, or opened in ADS by pressing Ctrl key and clicking the link in the comment section of the Cpu0_Main.c file (see line 37 in Figure 1).
Figure 1 Cpu0_Main.c file
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series