Community Manager

Community Manager
Jul 24, 2022
11:14 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: Using NC or NC1 balls for PCB routing - KBA235307
Version: **
There are two types of NC balls:
- NC: Not Connected. These pins are reserved for future extensions and shall not be connected externally.
- NC1: Not Connected. These pins are not connected at the package level and will not be used for future extensions.
The general rule is that NC and NC1 must not be connected to any net including power supply or ground connections in the PCB routing.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
- Tags:
- Board (PCB)
- package
Rate this article: